Hello,
I have created a simple multi-core project for RH850/U2A R7F702301A (292 pins)
I am able to build and download the code into the MCU but the code execution is halting at eiint24
I am not able to halt at r_cg_main for PE0
I tried to use the external table reference method but not successful
Can you please check the attached code and suggest
Also, share sample codes for this MCU for reference
BR,
Eshwar
Environment:
IDE: CS+ V8.10
Compiler CCRH V2.05.00
Host: Windows 11
MCU: R7F702301A (292 pins)
gdcu_platform.zip
The latest CS+ version 8.11 has some major fixes on interrupt handling. Please upgrade CS+ and try again.
Regards
Updated the IDE to V8.11 and freshly generated the code with smart configurator but still facing the same issue
Kindly suggest
What happens if you click on the Start button instead of Step in ?
If the start button is clicked, wait for some time and then click on stop button. Now the debugger is still pointing to the eiint24()
The execution has not moved further as I observed
Please check that this is the correct frequency of the main clock oscillator: