a. Customers ask us R7F701461 internal RAM 2 * 1.2M space utilization rate, seven-inch screen requirements are getting higher and higher whether it is enough;
b. Whether there is R7F701461 related models of demo board or can demonstrate the development board can be used, or whether there is a related instrumentation program video for them to watch for reference;
c.Whether the graphics library of this series MCU supports freetype font;
d.R7F701461EABE-C#BC0 to find out the external expansion can be connected to a maximum of 128MB of SDRAM, this kind of actual can be used in the graphics memory of the SDRAM is how much;
e.What tool is used for the graphics generation code and whether it is free;
f. Display RAM (both internal and external) how it is used, whether it supports multiple layers, multiple windows.
g.Will there be a CS+ version of the RGL library in the future for reference?
Biggest Thank You
Hi,
The RGL library can be found here: Renesas Graphics Library (RGL) | Renesas
Please contact us on our private ticket platform to discuss your requests in detailhttps://en-support.renesas.com/createticket
Best Regards,Vasanth