RH850/D1M1A Related Questions

a. Customers ask us R7F701461 internal RAM 2 * 1.2M space utilization rate, seven-inch screen requirements are getting higher and higher whether it is enough;

b. Whether there is R7F701461 related models of demo board or can demonstrate the development board can be used, or whether there is a related instrumentation program video for them to watch for reference;

c.Whether the graphics library of this series MCU supports freetype font;

d.R7F701461EABE-C#BC0 to find out the external expansion can be connected to a maximum of 128MB of SDRAM, this kind of actual can be used in the graphics memory of the SDRAM is how much;

e.What tool is used for the graphics generation code and whether it is free;

f. Display RAM (both internal and external) how it is used, whether it supports multiple layers, multiple windows.

g.Will there be a CS+ version of the RGL library in the future for reference?

Biggest Thank You

Parents Reply Children
No Data