DEEPSTOP MODE IMPLEMENTATION IN RH850 - R7F701686 MICROCONTROLLER

Hello,

          I am going to implement a deep stop mode in the RH850 microcontroller. What are the configuration I need to do manually to achieve the deep stop mode? It is not the same as the stop mode. I selected the deep stop mode and wakeup factor in the Smart Configurator. After generating the code, I followed the same procedure as for the stop mode, but the microcontroller does not enter the deep stop mode.

Thaks and Regards

Parents Reply Children