About Flash Memory CRC Operation Function (high-speed CRC) in the F23.

Hello. Renesas Team.

there are only two registers related to the high-speed CRC function: CRC0CTL and PGCRCL.
I understand that it works at the start of HALT instruction.
However, I do not expect detailed action.

The summary of my questions is as follows.

Q1. There is no register to know when the CRC calculation ended. Can I know the completion of the calculation?
Q2. Does the status transition automatically occur from HALT to NORMAL after the CRC calculation is completed?
Q3. If Q2's answer is no, should i wake up MCU at the expected end time(when CRC calculation is completed)?

Thanks