Hello,
I need to debug the code in CS+. Elf file is generated through windriver compiler. Controller used is RH850 E2GUH.
I am able to load the elf file in CS+ but download fails with the below error:
Download fail
[Direct error cause]Object reference not set to an instance of an object.
Please let me know how can I fix this issue.
Thanks
CS+ for RH850 family is supported by CC-RH compiler, Green Hills GHS RH850 compiler and the IAR RH850 compiler.
There is no support for Wind River compiler.