Hello.
If you look at the UM manual of RH850F1KM-S1 MCU,As you can see in the captured photo below,The difference between the Min/Max range of the sampling and conversion times in the A/D electrical specifications is written as being quite large.
The customer is requesting confirmation of the factors that cause the variation of the Min/Max times of each (Sampling, Conversion) Time.
1. Please answer why the variation range is so large.
Also, we received other question about whether there is a way to reduce the sampling and conversion time of AD. 2. If you have a solution or a method that you can suggest, please guide us by today.
Thank you.
Best Regards,
David lee.