Subject: Issue with SPI DMA Data Reception on RH850D1M1A - Code Goes to Reset Handler

Hello Team,

I am working on the RH850D1M1A with multiple GHS for our development. We are using SPI with DMA to receive data, and the data is correctly transferred into the DMA buffer. However, after the reception of data, the code unexpectedly jumps to the reset handler.