We use RL78/D1A 100Pin.How can I set up LIN Slave with Applilet3?PIN No. to be used.- PIN_35(P10/LTxD1/SCK00/TI10/TO10/INTP4/SEG31 ) : LIN TX- PIN_36(P11/LRxD1/INTPLR1/SI00/TI11/TO11/SEG30) : LIN RX- PIN_37(P12/SO00/TI12/TO12/INTP2/SEG29) : LIN ENable Pin
Hello,
The port registers should be set as following:
Also the STSEL0.SUARTF1 should be 0:
The LIN enable pin should be handled from GPIO so configuring it on Code Generator would be enough: