マイコン、初心者です。表題のターゲットボードを使用し、AD9833(信号発生器)にて信号を出力してみたいと思いいざ、プログラムを書いて実行してみるとまったく動いている気配がありません。クロック設定などはtargetboard for RX65N のボードサプライパッケージ?をダウンロードし使用しています。何が足りないのか、いろいろ分からないなりに調べつつ試している最中ですが動く気配がなく困っております、、汗何か、とんでもない欠陥や見落としがあると思うのですが、、どなたか、教えてください。コードとクロック設定やデバック構成などのスクショを添付しました。/cfs-file/__key/communityserver-discussions-components-files/395/rxdeAD9938.txt
AD9833のMCLKにクロックは供給されていますか?MCLKにクロック供給される回路構成のモジュール基板なら問題ないです。
ご回答ありがとうございます。はい、MCLKに水晶?から25Mhzクロック供給されるタイプのものです。こちらを使用しています。