PLEASE REFER TO THE APPLICATION NOTE FOR THIS MIDDLEWARE FOR MORE INFORMATION RX RSPI Driver ============== Document Number --------------- N/A Version ------- v1.40 Overview -------- Basic RSPI Master Mode driver. Features -------- * Functions to init, read, and write the RSPI channels * Ability to lock channels to a task to ensure no other tasks try to use peripheral while it is already being used. Supported MCUs -------------- * RX621, RX62N Group * RX630 Group * RX631, RX63N Group Boards Tested On ---------------- * RSK+RX62N * RDKRX62N * RSKRX63N * RDKRX63N Limitations ----------- * This code is not re-entrant but does protect against multiple concurrent function calls. Peripherals Used Directly ------------------------- * RSPI0 * RSPI1 * RSPI2 Required Packages ----------------- * none How to add to your project -------------------------- * Add src\r_rspi_rx.c to your project. * Add an include path to the 'r_rspi_rx' directory. * Add an include path to the 'r_rspi_rx\src' directory. * Configure middleware through r_rspi_rx_config.h. * Add a #include for r_rspi_rx_if.h to files that need to use this package. Toolchain(s) Used ----------------- * Renesas RX v1.02 File Structure: --------------- r_rspi_rx | readme.txt | r_rspi_rx_config.h | r_rspi_rx_if.h | \---src r_rspi_rx.c