I am using the P9235A-RB-EVK and the P9222-R-EVK to evaluate a non-standard coil configuration that results in an overall efficiency of 62% after tuning. I have it working pretty well, but when the load increases to where the input power is 4.0W to 4.2W, the transmitter goes into the "Power Limit" state.
There is no information in the datasheet as to what exactly triggers the "Power Limit" state? So what does trigger this state? It doesn't seem to be Over Current or Over Temperature, since those have their dedicated error states. Also, it doesn't seem to be tied to a certain input power value, since I can get past this limit by increasing the input voltage from 5V to 12V.
Also, is there a way for the Application Processor on the receiver side to determine what a 'safe' power draw would be?
Hello Martin,
Have you made any progress on this? I hope our experts can soon share their ideas on this thread.
All the best!
SaiRenesasRulz Forum Moderator
https://renesasrulz.com/ https://academy.renesas.com/ en-support.renesas.com/knowledgeBase