I need ISL85403 to work only in boost mode. Vin as low as possible, Vout = 16V.
I'm guessing highest range for Vin would be close to 16V, since there's no buck operation.
I came across the boost-buck circuit, which is "Figure 10. ISL85403EVAL3Z Schematic", taken in this application note.
Now, it has L1 22uH for buck converter side, right?
Can I just get rid of L1 and Q1 MOSFET then?
I only need the L2 6.8uH on Lgate and Vin for boost mode, correct?
Though I wanted to replace L2 with 10uH instead for better efficiency.
I have the iSIM PE, but couldn't figure out how to make sense of it.
Hi triedgetech,
For this device, please submit a Technical Support Inquiry: https://en-support.renesas.com/dashboard
JBRenesasRulz Forum Moderator
https://renesasrulz.com/https://academy.renesas.com/https://en-support.renesas.com/knowledgeBase/