m32r

Hello,

Can FDT version 4.09 write to mcu m32176? I mean cleaning the contents of this mcu.

Parents Reply
  • JimB, please tell me is it possible to connect to the MCU via the console and issue commands? According to the documentation, Block Erase (H'2020) is responsible for erase?
    Table 6.5.2 Commands in Flash E/W Enable Mode
    Command Name Issued Command Data
    Read Array command H'FFFF
    Halfword Program command H'4040
    Lock Bit Program command H'7777
    Block Erase command H'2020
    Clear Status Register command H'5050
    Read Lock Bit Status command H'7171
    Verify command (Note 1) H'D0D0

Children
  • I'm sorry I know nothing about these devices, I only have some experience with FDT and I knew where to find the info about which devices were supported, to answer your original question.

    Hopefully someone else would be able to help you with device specific questions.

    My advice would be if you are looking for hardware to use for educational purposes, to find something more recent.  For something like $25USD you can get a basic Renesas target-board for RX/RL78/RA that would have a full complement of tools available to use.  And I'm sure there a many other non-Renesas type of kits available at similarly low cost.

  • Thank you for the information provided. I will try to find a flash tool.