Target device : R7F701583
Connecting the toolTool : E1 emulator (9AS133910C), Interface : 2 wire UARTEmulator's supply power : OFFEmulator's firmware version:3.00.00.004Connecting to the target device
Disconnecting the toolError(E3000105): The device is not responding.Operation failed.
I am getting this error. I checked all the connections but still no use.
Performed E1 self test too. All the test cases are passing.
Please suggest something to get this issue resolved.
Niranjan,
What version of RFP are you using?
Have you checked that the target MCU has power?
Can you show the part of your schematic that shows your connections to the MCU?
Beside the already mentioned power supply, please check also that there is a working oscillator. Please check that you are using the latest version of the Renesas Flash Programmer (RFP: www.renesas.com/rfp). The recommended circuit for the programming and debugging interface can be found in the RH850/F1K E1/E2/E20 Addon Manual: R20UT3431EJ0400
Hi Fragero,
There is a issue with my hardware connections. fixed it now. Everything is working fine.
Thanks for the help.