Hi first time posting on the forums forgive me if this is the wrong group.So I installed the SuperH Compiler and I didn't see the Sega Dreamcast SH-4 Model listed in target devices page.
Can I request support for the dreamcast sh-4 and overlay support? thanks.
I suppose this was a customer specific device. This should not be a problem for the compiler as I guess it uses a standard SH-4 core, but you will not find the header files for the device or the debugger extensions as these were only provided to the customer.