P9415-R-EVK not changing to EPP mode

We received 2 samples of P9415-R-EVK to test for possible use in a new product we are designing. I am using a 10W transmitter with the P9415-R-EVK. I have followed the setup guide to the latter. I have tried changing the RX EPP mode parameters but I can't get it to go to EPP mode. I am able to get 10W when I change the RX BPP mode parameters. I have a 1A load connected. I have a screenshot with the current MTP settings and the reported values. Kindly assist.