Hi everyone,
I’m Darshan Hiranandani, looking into the different ldo_level_select settings for the DA7218, as detailed in the datasheet. The options range from 1.05 V to 1.40 V, but there isn’t much additional information about the benefits of selecting different values.
ldo_level_select
Does anyone have insights on whether there are advantages to using specific settings? For example, are there trade-offs between power usage and dynamic range that we should be aware of?
I’d appreciate any thoughts or experiences you might have regarding this!
Thanks!
Regards
Darshan Hiranandani
To best support you on this you will need to submit a Technical Support ticket by going to our support portal from the following link: https://en-support.renesas.com
You will need to sign in with your company email address, and if you don't have an account you will need to register with one. https://www.renesas.com/register
Best regards, Cindy, Renesas Online Applications Support Engineer