Darshan Hiranandani : How do varying ldo_level_select values impact the performance of the DA7218?

Hi everyone,

I’m Darshan Hiranandani, looking into the different ldo_level_select settings for the DA7218, as detailed in the datasheet. The options range from 1.05 V to 1.40 V, but there isn’t much additional information about the benefits of selecting different values.

Does anyone have insights on whether there are advantages to using specific settings? For example, are there trade-offs between power usage and dynamic range that we should be aware of?

I’d appreciate any thoughts or experiences you might have regarding this!

Thanks!

Regards

Darshan Hiranandani