D70F3180GJ V850E/GP2

Good afternoon
Is there a datasheet for D70F3180GJ V850E/GP2? I need to write the stock file to the processor. recording will be carried out using PG-FP5, PR5 file is available. From the processor pinout I only know the power supply - 5V and 2.5V (found on the board), quartz -16 MHz. For successful recording I want to know the location of the legs SCK SO SI RESET FLMD0...

thanks in advance!
Parents Reply
  • very sad if this is true...

    So, is it possible to replace the factory loader from Renesas with your own? why am I asking - I found a reset, flmd0, flmd1. 3 pins left. I went through these 3 pins in various combinations sck si so. the processor did not respond.. this suggests that the bootloader has been replaced) is this possible?

Children