D70F3180GJ V850E/GP2

Good afternoon
Is there a datasheet for D70F3180GJ V850E/GP2? I need to write the stock file to the processor. recording will be carried out using PG-FP5, PR5 file is available. From the processor pinout I only know the power supply - 5V and 2.5V (found on the board), quartz -16 MHz. For successful recording I want to know the location of the legs SCK SO SI RESET FLMD0...

thanks in advance!
Parents Reply
  • Pretty difficult to guess on this.  Ever device has built-in firmware for factory programming over a serial interface, but that can be disabled by the user.  Without device specifications it is impossible to know for sure which pins handle what functions.  I have noticed them many if not most devices do seem to share common pins, it might be possible to analyze other similar public V850 devices with similar packaging to guess which pins might work.

Children