Not able to record audio using ALSA on RZ/A1H board

Hi,

I am working on Renesas RZ/A1H platform with Linux Operating system.

I am trying to record audio using alsa with below command. 

$ arecord --format=S16_LE --rate=16000 --channels=1 test.raw -vv

The recorded audio has noise only. The audio codec is MAX9856 and I am using Audio-In port as "Audio Line-In". I have tried with all the different combination of sampling rate and channels but not able to record the voice. The configuration of Mixer is a default, I did not change any configurations. With default configurations of mixer, it is using LINEIN1 and LINEIN2 as input. I have tried with all different configuration but not able to record voice. The recorded audio has been tested with "aplay" command as well as with audio player in other systems after converting it into the required format.

When I use headphone as a recording device and insert headphone in Audio-In port then I was able to record voice from Audio-In port. (When I use headphone for recording I need to use earplugs to speak into it not microphone). Because of this scenario, I changed configurations of "Audio-In" port and make it as "Audio-Mic In" and change the required configurations with the use of "amixer" command but still not able to record the audio from the device. Can anyone please help me to record audio from "Audio-In" port of the device?

Please let me know if I need to put more information here for this issue. Looking forward to your support.

Thank you.

Parents
  • Hi Palak,

    Your issue is really broad. Aside from the RZ/A1H board, MAX9856 is another device to consider. If it's just fine with you, could you put more information like the schematics or how did you connect the devices and also the code or configurations you used? This will increase the chance for the forum to help you with your problem. Thanks!

    JB
    RenesasRulz Forum Moderator
Reply
  • Hi Palak,

    Your issue is really broad. Aside from the RZ/A1H board, MAX9856 is another device to consider. If it's just fine with you, could you put more information like the schematics or how did you connect the devices and also the code or configurations you used? This will increase the chance for the forum to help you with your problem. Thanks!

    JB
    RenesasRulz Forum Moderator
Children
  • Thanks for your response. I have configure Audio-In port as "Audio Mic-In" and change some required registers of codec and its working fine now. Thanks.
  • Oh that's great! Thanks for the response!

    JB
    RenesasRulz Forum Moderator
  • Hi ,

    I am using RZ/G1M and trying to record the audio using headphone but unable to record.

    root@skrzg1m:~# amixer scontrols
    Simple mixer control 'Headphone Enable',0
    Simple mixer control 'Playback ReConvert Rate',0
    Simple mixer control 'Capture ReConvert Rate',0
    Simple mixer control 'DVC In',0
    Simple mixer control 'DVC In Mute',0
    Simple mixer control 'DVC Out',0
    Simple mixer control 'DVC Out Mute',0
    Simple mixer control 'Digital',0
    Simple mixer control 'LINEOUT Mixer DACL',0
    root@skrzg1m:~#

    I could not see any LineIn to configure.

    Please let me know if I need to put more information here for this issue. Looking forward for support.

    Thank You