Hello,
I need your help.
I used thread monitor with WDT : working fine.
Now i wanted to move to IWDT : BIG ISSUE there is no reset, it seems that the timer doesn't work.
--------------------------------------------------------------------------------------
With WDT
R_DBG->DBGSTOPCR_b.DSWDT = 0;g_wdt0.p_api->open(g_wdt0.p_ctrl,g_wdt0.p_cfg); while(1);
The mcu reset -> working
With IWDT
R_DBG->DBGSTOPCR_b.DSIWDT = 0;g_wdt1.p_api->open(g_wdt1.p_ctrl,g_wdt1.p_cfg);while(1);
The mcu DOES NOT reset-> PLEASE HELP
I tried for a day without success
Thanks for your help
It works on an S5D9-PK for me. I changed the board to S5D9-PK, and made sure the iWDT Start mode is "IWDT is automatically activated after a reset (Autostart mode)" in the OFS register settings :-
and after about 20 seconds the code stops at the same point as before.