Hi,
I have a SK-S7G2. I initially used SSP V1.5.2 for a proof-of-concept. The experiment went well and now we have assembled our a hardware prototype based on SK-S7G2 but with subtle changes. Following have changed:
I had previously asked in a post on this forum itself about how to create a BSP for custom board, and it was answered to my expectations.
Now that I foresee a lot of application-level requirement changes, I am keen to know whats the recommended way of moving on with it.
My requirements are as follows:
I see that the SSP1.6.0 is released. Is it advised to begin with SSP 1.6.0 (and the official supported version of e2 studio for SSP 1.6.0)?
The question arises because there has been no documentation for creating a BSP for custom board using SSP V1.5.0 and an older document which guides about the process for SSP V1.2.0 onward, is no longer usable for e2 Studio V7.2.y or V7.1.y.
Please advice.