I am generating .txt files in a folder on a sdcard using FILEX. The problem is all the files created have a same timestamp of 01/01/2017. I had to create this files such that the latest file remains at the top of the folder while the oldest goes down automatically. It is same as sorting the folder by date in windows. How can i do it?. Can anyone help
Hi.
Here you should have all the information you need
https://renesasrulz.com/synergy/f/synergy---forum/17229/time-date-source-used-by-filex
Paolo
you can set the date and time for the files by using the code
fx_system_date_set ((UINT) ((g_system_time.tm_year - 100) + 2000), (UINT) g_system_time.tm_mon + 1, (UINT) g_system_time.tm_mday);
fx_system_time_set ((UINT) g_system_time.tm_hour, (UINT) g_system_time.tm_min, (UINT) g_system_time.tm_sec);