Hi,
e2Studio/SSP 7.5.1/1.7.8, S7G2
I have a working Thread-X application. I'm struggling with adding the simple serial bootloader to it. I've placed the image at 0x010200. The bootloader jumps to it just fine. However, as soon as I include the flash driver to the image HAL, the bootload jump fails with a stack error.
I'm confused as to what stack in the Thread-X application is affected by the addition of the flash driver to HAL. If one opens the configuration.xml file and selects BSP, the properties tab shows:
Main stack size, Process stack size, and Heap size
Is "main stack size" what is used by HAL?
Steve
No, each thread has it's own stack memory allocated. On a context switch, the PSP (Process Stack Pointer) is updated to point to the current stack location for that Thread in it's own stack memory area…