I created custom user pack for GT911 controller. It shows up in Stack list in Synergy Configuration
after adding and Generating Code source files are not added to Synergy folder.
where as existing pack for Controller FT5x06 is adding the source files.
I followed the instructions mentioned here
https://community.renesas.com/embedded-system-platform/synergy/f/forum/16491/create-cmsis-pack-for-touch-driver-gt911
I also tried adding source folder and files to the Synergy folder in the project and then exported pack file. still same issue.
this exported pack not showing in configuration.
any help please..
Hi path,
Can you check if this thread helps you with your issue: https://community.renesas.com/embedded-system-platform/synergy/f/forum/27754/include-files-from-ssp_supplemental-folder-inside-pack-file…
Can you check if this thread helps you with your issue: https://community.renesas.com/embedded-system-platform/synergy/f/forum/27754/include-files-from-ssp_supplemental-folder-inside-pack-file-not-found?
JBIf this response, or one provided by another user, answers your question, please verify the answer. Thank you!Renesas Engineering Community Moderatorhttps://community.renesas.com/https://academy.renesas.com/https://en-support.renesas.com/knowledgeBase/
I have gone through that thread earlier. everything looks fine at my end. for the workaround I copied the files to project directory manually. and when regenerating it is not deleting, so it is working for now. not tested the project on Target yet.
thanks for your support.