Avoid recompile when add ThreadX Source

I need to change some features of ThreadX in my project, so i added ThreadX as source. Because of that i need to recompile ThreadX each time i run clean, and this causes long compile time. After first build i do not change any configurations of the ThreadX, so there is no need for building ThreadX source each time i run clean. How can i add modified ThreadX build to project in Eclipse?

Parents Reply
  • I cant get the exact answer but seems like splittin project into 2 projects is the best way for me now. 1 for library project with all the configuration and synergy generated files and the other one for application code.

    Is there a way that i rebuild the ThreadX source with my configuration and pack it as a library? That way i dont need to clean and rebuild the ThreadX source everytime i run clean.

Children
No Data