Hi all,
We are working on:
s7g2 (Custom Board)
SSP 1.7.0
e2Studio 7.8.0
API: Netx Duo.
The activities in IP Stack:
1. WebServer, (User Login)
2. TCP/IP Server (Periodical)
3. imcp (ping test for gateway link) (Periodical)
In few cases we find that the IP Tasks (mentioned above) stop working completely.
No Response to ping,
Webserver Login page does not load,
TCP/IP Server does not respond.
However other non-IP related tasks such as OLED etc are still running (Not a crash)
Any idea what can cause this?
There is no timeline as to when it occurs, 1hr, 1 day, 1 week...
I went through a lot of related threads.
One of which is very similar to my condition:
https://community.renesas.com/embedded-system-platform/synergy/f/forum/17295/ip-instance-stops-working-ssp-1-7-12
Is it because of High Traffic Network.
I hope Renesas Team can shed some light on it.
Regards,
Surojit
Hi Surojit,sry for the late response... The attached project has a network monitor thread, that waits for an event flag to be set by the PTP MINT interrupt callback, it unitialises the Ethernet link in…
Hi All,
Does anybody have a lead on this?
Please share if so.