Sigma Delta ADC Differential input disconect detection

Hi all,

I am using R7FS1JA783A01CFM microcontroller with 4 sigma delta differential adc channels from SD00-03 (4 channels)  with 4 termocouples. Each Termocouple has the next design in order to have 3V in the entry of the positive side to get the signal to saturation in case the sensor has been broken.


However, the value is the same as if the termocouple was without voltage or with 0 degrees. The desing seems to be okey but the signal value is not. I have been checking the manual and I get to I get to the paragraph "33.3.11 Disconnection Detection Assist Function" however the solution seems similar to what i proposed but using a single ended entry.

Why I am not seing the result in saturation if I have 3V in the entry of the disconected sensor?

Parents
  • When calibrating the SDADC24, the differential input voltage must be in the range shown :- 

     

     

    With 3V in CHnP and 0V in CHnN, the differential input voltage will be outside the range allowed for calibration.

     

    Calibration must be performed when using differential input mode, the first time after a reset (or stored calibration values loaded) :- 

     

    That´s why when we use calibration in the ssp it is not working properlly. If we deactivate it, it works without problems.
    -------------------------------------------------------------------
    The response was given by the Renesas Customer Hub.

Reply
  • When calibrating the SDADC24, the differential input voltage must be in the range shown :- 

     

     

    With 3V in CHnP and 0V in CHnN, the differential input voltage will be outside the range allowed for calibration.

     

    Calibration must be performed when using differential input mode, the first time after a reset (or stored calibration values loaded) :- 

     

    That´s why when we use calibration in the ssp it is not working properlly. If we deactivate it, it works without problems.
    -------------------------------------------------------------------
    The response was given by the Renesas Customer Hub.

Children
No Data