Hi, I'm making a custom bootloader based on this project https://en-support.renesas.com/knowledgeBase/19641190. But want to adapt it to work with the "Bootloader Firmware Image External Framework".
I'm guessing I have to modify the CRC builder since it point to the partitioned memory for the project
But don't know to where it should be pointing
Can someone give some pointers? (pun intended)
Hello Chalo1304,
Take a look on the project below:
https://github.com/IanHallRenesas/YASB_S5D9_Public
It is called YASB (Yet Another Synergy/Secure Bootloader). This is different to the Flashloader as the Flashloader has no authentication other than a simple CRC. YASB is much less complex than the SBM.
It has been written for the Synergy S5D9 MCU and published it publicly on GitHub. It uses the same concept as MCUBoot on RA. That is, images are signed for authentication and integrity purposes. Porting this to the S7G2 should not be difficult.
Regards,
AL_Renesas
Hi AL_Renesas
I had checked it before but dropped it since I couldn't even built it.
.eclipse\com.renesas.platform_1130179900\Utilities\\/isdebuild: not found
Do you know what could be causing this?. Could be cause the project was with 2.0.0 version?.
Thanks
I apologize for the delay,
A Field Application Engineer will support you directly.