Multiple ADC channels with some incorrect value

Hi,

I'm using S7A3 MCU, SSP 2.4.0

Trying to measure 16 analog input using ADC14. The ADC read that return few channel is lower than other. I measure the voltage at the ADC input pins and it has the same voltage as other input. my code is below

    volatile bool               adc_convert_complete = false;
    uint16_t                    adcBuffer[16];
    adc_register_t              adcChannel[] = {ADC_REG_CHANNEL_0, ADC_REG_CHANNEL_1, ADC_REG_CHANNEL_2,
                                            ADC_REG_CHANNEL_3, ADC_REG_CHANNEL_4, ADC_REG_CHANNEL_5,
                                            ADC_REG_CHANNEL_6, ADC_REG_CHANNEL_7, ADC_REG_CHANNEL_8,
                                            ADC_REG_CHANNEL_16, ADC_REG_CHANNEL_17, ADC_REG_CHANNEL_18,
                                            ADC_REG_CHANNEL_19, ADC_REG_CHANNEL_20, ADC_REG_CHANNEL_21,
                                            ADC_REG_CHANNEL_22};
    
    g_adc0.p_api->open(g_adc0.p_ctrl, g_adc0.p_cfg);
    
    R_S14ADC->ADHVREFCNT_b.HVSEL = 1;
    R_S14ADC->ADHVREFCNT_b.LVSEL = 1;
    R_S14ADC->ADCSR_b.ADHSC = 0;            // High speed A/D conversion
    R_S14ADC->ADSSTR0n_b[0].SST = 38;
    R_S14ADC->ADSSTRO_b.SST = 38;
    
    status =  g_adc0.p_api->scanCfg(g_adc0.p_ctrl, g_adc0.p_channel_cfg);
    
    while(1)
    {
        g_adc0.p_api->scanStart(g_adc0.p_ctrl);

        while (adc_convert_complete == false);           
        adc_convert_complete = false;                    

    
        for (int i = 0; i < 16; i++)
        {
            g_adc0.p_api->read(g_adc0.p_ctrl,  adcChannel[i], &adcBuffer[i]);
        }
        g_adc0.p_api->scanStop(g_adc0.p_ctrl);
    
        tx_thread_sleep (100);
    }

void mcu_adc_callback (adc_callback_args_t *p_args)
{
    SSP_PARAMETER_NOT_USED(p_args);
    adc_convert_complete = true;
}

The conversion is show below: Channels in green boxes are measured that all having the same voltage input. However, couple channels with red arrows are reading lower than others. The channels with read arrows read correctly when I significantly lower  the input voltage level.

Is there anything I did wrong? Does it require to be calibrated (how)

Thanks,

Parents Reply
  • Hi, Jayesh,

    Inputs into the ADC are buffered with Opamp in series with 10K resistor or some voltage divider which is less than 10K. I don't think 10K is very impedance. Can you verify if this is the case for the S3A7. 

    In one of your replies, you mentioned about different impedance. If I have one channel input impedance is 10k but other is 5k Ohm, is this would cause the issue?  

       

Children