Hi All,
Original Post by me:
https://community.renesas.com/mcu-mpu/embedded-system-platform/f/forum/29322/ip-tasks-do-not-respond-after-an-arbitrary-period-of-time
Related threads viewed:
https://community.renesas.com/embedded-system-platform/synergy/f/forum/17295/ip-instance-stops-working-ssp-1-7-12
https://community.renesas.com/mcu-mpu/embedded-system-platform/f/forum/14492/netx-packet-pool-depletion/111974#111974
Platform:
Version: 2022-04 (22.4.0)Build Id: R20220331-2313
SSP: v2.3.0
S7DK
Problem:
We are running MODBUS TCP Slave Server in a thread. The send and receive pool are different. After some time we find that the pool used for sending/replying is getting depleted.
Please feel free to ask for any relevant information. (Wireshark/source code etc.)
I have included the receive/send code with this post.
static BOOL _FnMODBUSTCPSlave(uint16_t u16NoMBSlaveClients, BOOL bMBSlaveFirst) { BOOL bCmdBC = FALSE, bCmdValid = FALSE; ULONG ulactual_events = 0, ulMBSlaveMsg[2], utcp_bytes_received = 0, uStatus = 0;//,ulfree_packets=0; UINT uiStatus = 0, uiStatusRetrv = 0,uiStatusRetrvLenCheck=0; //,uiStatusReles = 0; uint16_t u16MsgTransLen = 0, u16RplyMsgsizeL = 0, u16SocketCheckCtr = 0,u16TCPSendError=DEF_TCP_SLAVE_REPLY_ERROR_NONE; NX_TCP_SOCKET *socket_ptr = NULL; NX_PACKET *pMB_RX_packet_ptr = NULL; NX_PACKET *pMB_TX_packet_ptr = NULL; uint16_t u16NoUsedSoc = 0; StructMBSlaveCmdExeParams *pMBSlaveCmdExeParams = &sMBSlaveTCPCmdExeParams; sMBSlaveTCPCmdExeParams.CmdOffset = 6; uint8_t *pMODBUSSlaveCmdRcv = sMBSlaveTCPCmdExeParams.MBReceiveFrame,u8PoolFreeCtr=0; uint8_t *pMBTranReplyFrame = sMBSlaveTCPCmdExeParams.MBReplyFrame; StructMBSlaveClientParam *pMBSlaveClientParam = NULL; //ssp_err_t g_MBSlave_ip_io_pool_err = SSP_SUCCESS; sMODBUSSlaveOpr.bMBSlaveSts = TRUE; sLogMODBUSComm.bMODBUSPoolDepleted=FALSE; sLogMODBUSComm.bIPPoolDepleted=FALSE; /* Start listening on the first available socket */ FnSetMBSlaveStartSocketListen (); tx_timer_activate (&Timer_MBSlaveClientStatusCheck); while ((uiStatus = tx_event_flags_get (&EvDevInConfig, EV_FLAG_DEVICE_IN_CONFIG, TX_AND, &ulactual_events, TX_NO_WAIT)) == TX_NO_EVENTS) { uiStatus = tx_queue_receive (&QMBSlave, ulMBSlaveMsg, TX_NO_WAIT); if (TX_SUCCESS == uiStatus) { // MBSlave message received . process the same socket_ptr = (NX_TCP_SOCKET*) ulMBSlaveMsg[0]; pMB_RX_packet_ptr = (NX_PACKET*) ulMBSlaveMsg[1]; if (socket_ptr != NULL && pMB_RX_packet_ptr != NULL) { pMBSlaveClientParam = _FnMBSlaveFindClient (socket_ptr); if (pMBSlaveClientParam != NULL) { utcp_bytes_received = 0; //Check Rcv Msg Length uiStatusRetrvLenCheck = nx_packet_length_get(pMB_RX_packet_ptr,&utcp_bytes_received); if(uiStatusRetrvLenCheck==NX_SUCCESS && utcp_bytes_received<MAX_MODBUS_SLAVE_MESSAGE_RCV_LEN) { //Length is within limit uiStatusRetrv = nx_packet_data_retrieve (pMB_RX_packet_ptr, pMODBUSSlaveCmdRcv, &utcp_bytes_received); } else { //Cannot retrieve. utcp_bytes_received=0; } nx_packet_release(pMB_RX_packet_ptr); u16MsgTransLen = 0; bCmdValid = FALSE; //Get Client Socket Status. nx_tcp_socket_info_get (&pMBSlaveClientParam->NX_TCPServerClientSocket, 0, 0, 0, 0, 0, 0, 0, &uStatus, 0, 0, 0); if ((NX_TCP_ESTABLISHED == uStatus || NX_TCP_SYN_RECEIVED == uStatus) && (uiStatusRetrv == TX_SUCCESS && utcp_bytes_received > 0)) { tx_event_flags_set (&EvMBTCPSlaveClientConnected, pMBSlaveClientParam->EvMBSlaveClientConnected, TX_OR); //Command Recvd Process the same.. if (_FnMODBUSTCPSlaveValidateCmd (pMODBUSSlaveCmdRcv, utcp_bytes_received)) { bCmdValid = TRUE; pMBSlaveCmdExeParams->MBSlaveAddr = pMODBUSSlaveCmdRcv[6]; //MB Slave address bCmdBC = FALSE; if (pMBSlaveCmdExeParams->MBSlaveAddr == 0) { bCmdBC = TRUE; } pMBSlaveCmdExeParams->RcvMBSlaveCmd = pMODBUSSlaveCmdRcv[7]; //Reset MODBUSReplySend to FALSE pMBSlaveCmdExeParams->bMODBUSReplySend = FALSE; pMBSlaveCmdExeParams->bIllegalAddr = FALSE; //Parse the message and get its response. FnMBSlaveComdExe (pMBSlaveCmdExeParams, bCmdBC); if (pMBSlaveCmdExeParams->bIllegalAddr == TRUE) { //Create message for illegal address. FnMBSlaveExcepResp (DEF_MB_ILLEGAL_DATA_ADDRESS, pMBSlaveCmdExeParams); } if (pMBSlaveCmdExeParams->bMODBUSReplySend) { u16RplyMsgsizeL = pMBSlaveCmdExeParams->RplyMsgsize; pMBTranReplyFrame[0] = pMODBUSSlaveCmdRcv[0]; //???? Cast using uchar or make both uint8_t pMBTranReplyFrame[1] = pMODBUSSlaveCmdRcv[1]; pMBTranReplyFrame[2] = pMODBUSSlaveCmdRcv[2]; pMBTranReplyFrame[3] = pMODBUSSlaveCmdRcv[3]; pMBTranReplyFrame[4] = (uint8_t) ((u16RplyMsgsizeL) >> 8); pMBTranReplyFrame[5] = (uint8_t) ((u16RplyMsgsizeL) & 0x00FF); u16MsgTransLen = (uint16_t) (pMBSlaveCmdExeParams->RplyMsgsize + 6); u8PoolFreeCtr=0; do { // Set Send Timeout Option Place data in the packet. uiStatus = nx_packet_allocate (&g_MBSlave_ip_io_pool, &pMB_TX_packet_ptr, NX_TCP_PACKET, 100); if(uiStatus == NX_SUCCESS) { break; } u8PoolFreeCtr++; tx_thread_sleep (100); } while (uiStatus != NX_SUCCESS && u8PoolFreeCtr < DEF_POOL_FREE_CHECK_COUNT_NO); u16TCPSendError = 0; if (uiStatus == NX_SUCCESS) { sLogMODBUSComm.bMODBUSPoolDepleted=FALSE; uiStatus = nx_packet_data_append (pMB_TX_packet_ptr, pMBTranReplyFrame, (ULONG) (u16MsgTransLen), &g_MBSlave_ip_io_pool, NX_NO_WAIT); if (uiStatus == NX_SUCCESS) { uiStatus = nx_tcp_socket_send(socket_ptr, pMB_TX_packet_ptr, 100); if (uiStatus != NX_SUCCESS) { uiStatus = nx_packet_release(pMB_TX_packet_ptr); if (uiStatus != NX_SUCCESS) { u16TCPSendError = DEF_TCP_SLAVE_REPLY_ERROR_POOL_RELEASE_FAIL_SEND; } else { u16TCPSendError = DEF_TCP_SLAVE_REPLY_ERROR_SEND_FAIL; } } } else { uiStatus = nx_packet_release(pMB_TX_packet_ptr); if (uiStatus != NX_SUCCESS) { u16TCPSendError = DEF_TCP_SLAVE_REPLY_ERROR_POOL_RELEASE_FAIL_APPEND; } else { u16TCPSendError = DEF_TCP_SLAVE_REPLY_ERROR_APPEND_FAIL; } } } else if(!sLogMODBUSComm.bMODBUSPoolDepleted) { sLogMODBUSComm.bMODBUSPoolDepleted=TRUE; FnAddFaultLog (DEF_FAULT_MBSLAVE_TRANS_POOL_DEPLETE); } } } if (sLogMODBUSComm.bMODBUSTCPSlaveLog) { FnMODBUSCommMonLog (pMBSlaveClientParam->u16MBSlaveClientID, pMODBUSSlaveCmdRcv, utcp_bytes_received, pMBTranReplyFrame, u16MsgTransLen, bCmdValid, u16NoUsedSoc, u16TCPSendError, uiStatus,sLogMODBUSComm.bMODBUSPoolDepleted,en_COMM_OK_RESP_VALID); } } else if (sLogMODBUSComm.bMODBUSTCPSlaveLog) { FnMODBUSCommMonLog (pMBSlaveClientParam->u16MBSlaveClientID, pMODBUSSlaveCmdRcv, utcp_bytes_received, pMBTranReplyFrame, 0, FALSE, u16NoUsedSoc, DEF_TCP_SLAVE_REPLY_ERROR_SOCKET_NOT_AVAILABLE, 0,sLogMODBUSComm.bMODBUSPoolDepleted,en_COMM_FAIL); } } else { nx_packet_release(pMB_RX_packet_ptr); } } else if (pMB_RX_packet_ptr != NULL) { nx_packet_release(pMB_RX_packet_ptr); } } tx_thread_sleep (6);//(10); //Check Client Socket Status //Uncomment Later 29.06.2022 u16SocketCheckCtr++; if (u16SocketCheckCtr >= DEF_SOCKET_MON_TIME_SEC) { u16SocketCheckCtr = 0; if ((tx_event_flags_get (&EvMBSlaveClientStatusCheck, EV_FLAG_TIMER_MBSLAVE_CLIENT_STATUS_CHECK, TX_AND_CLEAR, &ulactual_events, TX_NO_WAIT)) == TX_SUCCESS) { u16NoUsedSoc = FnMBSlaveTCPClientSocketStatusCheck (u16NoUsedSoc); } } } sMODBUSSlaveOpr.bMBSlaveSts = FALSE; tx_timer_deactivate (&Timer_MBSlaveClientStatusCheck); SSP_PARAMETER_NOT_USED(u16NoMBSlaveClients); bMBSlaveFirst = FALSE; return bMBSlaveFirst; }
I need a solution ASAP,
Thanks for your help in advance.
Regards,
Surojit
Hello,
I cannot think of anything else other than increase the pool size.
Regards
Hi Surojit.Apologies for the delay. We've escalated both the issues posted by you to an internal team. They'll reach out to you. Thanks for your patience.Regards,Jayesh
Thank You Jayesh,
Please keep me posted.
Feel free to ask for any details.
Surojit.
I have increased the pool to 200, however this pool also depletes after 36 to 48 hours. We need to know why the pool depletes and how to prevent it. Increasing pool size is not the solution.
Please check and advise further.
Thanks