eMMc JEDEC version 5.1

Hi All,

We are Using:

Platform:

Version: 2022-04 (22.4.0)
Build Id: R20220331-2313

SSP: v2.3.0

S7DK

Problem:

We want to use 16GB eMMC all of which use a JEDEC v5.0/5.1.

when we use such a chip in our system it does not work.

We are using SSP 2.3.0

Any Clues?

Regards,

Surojit

Parents Reply
  • You should talk to the part vendor - my understanding is that if the driver only uses jedec 4.52 features, a 5.0 part should work.  Or you could add the jedec 5.0 support yourself - the vendor may have a block driver, or you could mod the one from the linux tree for ThreadX.  So what doesn't work? Can you ID the part, check size, etc? Something must work unless the connection is different

Children