Selection of MCU - SD24 - Weight Scale

I need help with MCU Selection.

The main aim is to replace (STM8s and HX711) Chips in a weight scale project.

So, it should be low in cost, the SD24 PGA Gain should be 128.

Note: Load cell maximum weight could be greater than 200kg.

Parents Reply Children
No Data