Hello,
I want to get the unique id in the s5d9 mcu, I use g_fmi_on_fmi.uniqueIdGet(&p_unique_id), using this api I can get the id successfully, but when I check the ssp user manul 2.4.0,
4.2.22.3 FMI HAL Module Operational Overview
it said “For the S5D9 MCU, the fmi_api_t::uniqueIdGet API returns an error. There is no workaround."
Why i didn't get the error? it return 0, whitch means sucess
I think it is fixed in v2.5.0 version.
Using the PK-S5D9 and this application I don't see an error.
PK_S5D9_uniqueID.zip
Hi Michael,
I didn't see error too, my question is why the ssp user manul give a different result as below: