When using the QSPI driver to store data with GUIX Studio, the image is not displayed on the screen

I'm using a custom board based on the S7G2 PE-HMI Kit. I created a BSP based on the BSP available from other Kits for an ISSI memory, with the GUIX resources stored in the microcontroller's internal memory. I did all the tests following the manuals and writing and reading occur correctly, however when starting the QSPI driver, no image appears on the screen. I need to use this external QSPI memory to store data only.