I'm using a custom board based on the S7G2 PE-HMI Kit. I created a BSP based on the BSP available from other Kits for an ISSI memory, with the GUIX resources stored in the microcontroller's internal memory. I did all the tests following the manuals and writing and reading occur correctly, however when starting the QSPI driver, no image appears on the screen. I need to use this external QSPI memory to store data only.
Hi Digimed.It could be that the QSPI has not been set up correctly. Please check out the following thread, where Jeremy has described a method to check the proper initialization of QSPI. Let us know if it is helpful.https://community.renesas.com/mcu-mpu/embedded-system-platform/f/forum/15959/guix-does-not-work-with-resouces-in-qspi/51310#51310Regards,Jayesh If this response, or one provided by another user, answers your question, please verify the answer. Thank you!Renesas Engineering Community Moderatorshttps://community.renesas.com/https://academy.renesas.com/en-support.renesas.com/.../