redirecting printf

Hi 

at the moment iam working with the Renesas DK-S7G2 my printf function succesfully posts on the renesas virtual debug console. The problem here is the console is connected with COM1 how can i change this console to connect with a another COM port. The reason i wanna change this is because i implemented a UART connection and the UART connection is using the COM1. So this means that the debug console will not receive anything anymore is there a work around so i can use UART + the virtual debug console.

Parents Reply Children
No Data