I am currently using SSP v2.2.0 and am facing an issue with USB Mouse, cursor is not shown if I am using Screen Rotation(Although I can see via debug that the mouse co-ordinates being updated). Is there any workaround to it ? If anyone has come across this issue or knows something please help.
So I wanted to see the release notes for all the SSP version from 2.3.0 to 2.6.0 to see if any updates have been provided for the same and if so then I can consider updating to the latest SSP.
If I can get access to the release notes for these version 2.3.0 to 2.6.0 will be helpful. Thankyou.
Hello,
Here are the SSP release notes:
r11ut0089eu0102-synergy-sspv230-rel-note.pdf
r11ut0092eu0101-synergy-sspv240-rel-note.pdf
r11ut0095eu0101-synergy-sspv250-rel-note.pdf
www.renesas.com/.../ssp-260-release-note