I upgraded from 2022-04 to 2024-07. In doing so, the IDE no longer programs QSPI when I debug my application. It will program the internal FLASH of the device.
================ BUILD ===========================Extracting support files...14:12:46 **** Incremental Build of configuration Debug for project PROJ ****make -r -j8 all arm-none-eabi-size --format=berkeley "PROJ.elf" text data bss dec hex filename2456180 11471872 20852832 34780884 212b6d4 PROJ.elf14:12:47 Build Finished. 0 errors, 0 warnings. (took 1s.916ms)================== DEBUG =========================GDB Server for Renesas targets. Version 9.6.0.v20240708-130119 [c3334318] (Jul 10 2024 12:31:49)Starting server with the following options: Raw options : C:\Users\<user>\.eclipse\com.renesas.platform_510646852\DebugComp\\Synergy\e2-server-gdb -g SEGGERJLINKARM -t R7FS7G27H -uConnectionTimeout= 30 -uSelect= USB -uJLinkSetting= C:\Projects\ngt\ngt_1_A\src/NGT app.jlink -uJLinkLog= C:\Projects\ngt\ngt_1_A\src/JLinkLog.log -uLowPower= 0 -uInteface= SWD -uIfSpeed= 4000 -uResetBeginConnection= 1 -uNoReset= 1 -uResetPreRun= 1 -uIdCodeBytes= FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF -uDisconnectionMode= 2 -uSWOcoreClock= 0 -uresetOnReload= 1 -n 0 -uFlashBp= 1 -uSimulation= 0 -ueraseRomOnDownload= 0 -ueraseDataRomOnDownload= 0 -uOSRestriction= 0 -uAllowCachingFlash= 1 -uCPUFrequency= 0 -uCECycle= 1 -uResetBehavior= Reset -l -uCore= SINGLE_CORE|enabled|1|main -uSyncMode= async -uFirstGDB= main --english --gdbVersion= 12.1Using J-Link version V7.84d - C:\Users\<user>\.eclipse\com.renesas.platform_510646852\DebugComp\Synergy\ARM\Segger\JLinkARM.dllConnecting to R7FS7G27H, ARM Target GDBServer endian : little Target power from emulator : Off Starting target connectionFinished target connectionGDB: 4580Target connection status - OKTarget connection status - OKStarting downloadOption Function Select, writing to address 0x00000400 with data fffffffffffdffffSECMPUxxx, writing to address 0x00000408 with data ffffffffffffffffffffffffffffffff...Finished downloadGDB action 'Finished download', has failed with error report, failed to download