Ethernet Flash Boot Loader

Hi guys,

I just started to build an app on PE-HMI1 (SSP 1.2.1).

I want know if there are some example of BootLoader work on ethernet like the old RX62N/RX63N ( www.renesas.com/.../D3007836.html )

Somebody knows something already implemented.

Thank you.

Parents Reply
  • Hi Microit,

    Did you copy the Renesas.Synergy_flashloader.1.2.0-b.1.pack file to %E2_STUDIO_DIRECTORY%\internal\projectgen\arm\Packs from Flashloader_DK_S7G2.zip\Flashloader_Module?

    As Karol said, the project was developed for SSP 1.2.0-beta.1, but should work on SSP 1.2.0 as well.

    Regards,
    adboc
Children