Hello,
I've been playing around the the AE-CLOUD2 demo board and various demo applications provided. I've run the pre-compiled binary that connects to the Demo Dashboard, and also built the Synergy MQTT/TLS AZURE CLOUD CONNECTIVITY application project, but the Azure project doesnt send the same information that the Demo project does. Is the source code for the demo project available anywhere?
Also, there has been some mention on these forums of people spinning their own dashboards based off of sample code; is that sample code still available?
Thanks!