set value to GTCCRA and GTCCRB to generate a saw-wave PWM (RA6M3)

hi,

i'm studying RA6M3 for a potential project. I intend to use GPT to generate a PWM. I studied the FSP configurator, select a GPT module, it looks OK, user can set the  duty cycle for a PWM waveform.

but my application will be a saw-wave PWM, so I need to set value to GTCCRA and GTCCRB. but I didn't find where i can set the value for these two registers with FSP configurator? I may have to do it by directly writing registers in my code? 

appreciated for your help.

Parents
  • The initial values for GTCCRA / GTCCRB are set via the "Duty Cycle Percent" parameter.

     

    This will set the GTCCRA / GTCCRB to the same value.

     

    During your application, the GTCCRA / GTCCRB registers can be set with the API call R_GPT_DutyCycleSet(), for example:

        err = R_GPT_DutyCycleSet(&g_timer3_ctrl, 0x1234, GPT_IO_PIN_GTIOCA);
        if( err != FSP_SUCCESS )
        {
            __BKPT(1);  // error - investigate why.
        }
        
        err = R_GPT_DutyCycleSet(&g_timer3_ctrl, 0x5678, GPT_IO_PIN_GTIOCB);
        if( err != FSP_SUCCESS )
        {
            __BKPT(1);  // error - investigate why.
        }

Reply
  • The initial values for GTCCRA / GTCCRB are set via the "Duty Cycle Percent" parameter.

     

    This will set the GTCCRA / GTCCRB to the same value.

     

    During your application, the GTCCRA / GTCCRB registers can be set with the API call R_GPT_DutyCycleSet(), for example:

        err = R_GPT_DutyCycleSet(&g_timer3_ctrl, 0x1234, GPT_IO_PIN_GTIOCA);
        if( err != FSP_SUCCESS )
        {
            __BKPT(1);  // error - investigate why.
        }
        
        err = R_GPT_DutyCycleSet(&g_timer3_ctrl, 0x5678, GPT_IO_PIN_GTIOCB);
        if( err != FSP_SUCCESS )
        {
            __BKPT(1);  // error - investigate why.
        }

Children