This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Will a debugger prevent entering Deep Software Standby?

I'm using an RA6M3 connected to IAR's EWARM IDE via a J-Link Ultra+. I've read the Low Power Mode section of the RA6M3 user's manual and have looked at the register values and I think I have everything configured correctly. However, when I single-step through my code, it just steps right over the WFI instruction. I would expect the WFI to never return. The debugger would only resume after the device has reset out from the deep software standby state.

Before I pull out more hair, I thought I'd check to see if it is the debugger itself that is preventing the RA6M3 from entering deep software standby.




[locked by: Sai (SWF) at 12:32 (GMT 0) on 17 Nov 2022]
Parents Reply Children
No Data