Hello,
I'm implementing FreeRTOS in RA6T2 for the project, and now I have a question about the low power mode,
according the rm_freertos_port_sleep_preserving_lpm (uint32_t xExpectedIdleTime) in rm_freertos_pot/port.c
/** Check if the LPM peripheral is set to go to Software Standby mode with WFI instruction. * If so, change the LPM peripheral to go to Sleep mode. */
if (R_SYSTEM_SBYCR_SSBY_Msk & saved_sbycr) { /* Save register protect value */ uint32_t saved_prcr = R_SYSTEM->PRCR;
/* Unlock LPM peripheral registers */ R_SYSTEM->PRCR = RM_FREERTOS_PORT_UNLOCK_LPM_REGISTER_ACCESS;
/* Clear to set to sleep low power mode (not standby or deep standby) */ R_SYSTEM->SBYCR = 0U;
/* Restore register lock */ R_SYSTEM->PRCR = (uint16_t) (RM_FREERTOS_PORT_LOCK_LPM_REGISTER_ACCESS | saved_prcr); }
I'm wondering if the sleep mode is the one and only LPM can be used in FreeRTOS?
Can I enter Software Standby mode in the project using FreeRTOS?
Thanks.
Hi Cooper,
While looking for information, I found this app note and in chapter 3.2, it say there that "The LPMapplications do not use RTOS". I'm not sure about it. I hope someone from the RA team can…