RA6E1 or RA4E1 USB Example

Hallo,

i evaluate for a new project the RA[4/6]E1 Controllers.

I have some problems to find a working USB sample. Currently i have a fpb_ra6e1 board here. 

In the board examples folder https://github.com/renesas/ra-fsp-examples/tree/master/example_projects/fpb_ra6e1 is no USB sample. 

I modified the sample:

https://github.com/renesas/ra-fsp-examples/tree/master/example_projects/ek_ra6m1/usb_phid/usb_phid_ek_ra6m1_ep 

https://github.com/renesas/ra-fsp-examples/tree/master/example_projects/ek_ra4m1/usb_phid/usb_phid_ek_ra4m1_ep

to work with the R7FA6E10F2CFP Controller. But nothing (USB) is working.

I have Connected USB-DP, USB-DM and USB_VBUS to P407. Adjusted the USB Clock to 48 MHz. 

Is a demo HID, CDC, WINUSB is available to evaluate the USB functions?

Parents Reply
  • Thank you. The the USB demo is now working.

    With freertos is a composite device demo included (usb_composite_ek_ra6m1_ep) - this is working. With threadx (usbx) no sample or a demo with a compsite device is avalilable.

    Is it possible to use the USBX stack with a composite device (hid+cdc)?

    Exist a manual how to implement a own interface (Custom usb device interface) with usbX?

Children