Hello all,
I am looking the way to make function returns number of milliseconds since restart, same functionality as millis() in Arduino world.
Using e2 Studio, micro is R7FA6T1AD3CFM.
I have tried such function, see below, but it works only under debugger, otherwise (DWT->CYCCNT) returns constant so whole function also returns constant.
Are there any solution?
uint32_t millis() { uint32_t res = R_FSP_SystemClockHzGet(FSP_PRIV_CLOCK_PCLKD); //get system clock in Nz res = res / BSP_DELAY_UNITS_MILLISECONDS; //convert to kHz res = (DWT->CYCCNT) / res; //get #of cycles and convert to mS return res; }
Not a problem, I will leave as it is now, with extra GPT timer.