RA6M2 pcdc operation mode file.

Hello,

I am using pcdc mode and I can not locate the r_usb_pcdc_apl_config.h file. The reason for finding this file is that I want to change the USB_PCDC operation mode from ECHO_MODE to UART_MODE so that I can complete my project.

There is one more query is that, how can I sense and manage the usb hmsc mode and usb pcdc mode. I tried using it by sensing the VBUS and in this the default mode is hmsc mode and once I open the freertos_fat I can not close it if it is not connected, if I do it get crash.