This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

SSEL

This applies to a RA4M1 but I suspect other devices are similar.

How do I determine whether SSEL remains asserted while more data is sent or it is negated when the current data transmission completes?

For example: M95M01 and other serial EEproms require SSEL to remain asserted whilst an entire page of data is read or written.




[locked by: Sai (SWF) at 12:48 (GMT 0) on 2 Feb 2023]
  • Hi Ian,

    Thanks for your question on Renesas Engineering Community.

    Some RA devices support SSL Signal Level Keeping in order to implement a burst transfer like in EEPROM access. If this function is supported, bit 7 of SPCMD register should be set to 1 (for example in RA6M3 ). 

    However this setting is not available for RA4M1 as there is not such an option.

    Let us know if you have more questions.

    Regards,

    AZ

  • That seems rather final!

    I'd better write some code to set and clear SSEL.